ACTION#.RUNCOUNT
Description
This keyword displays the number of times an action ran since the time the Action was activated. It does not take any arguments. When an Action is activated, it automatically clears this count. The count value is only available for edge-triggered tasks and not for continuous tasks.
Examples
Code
--> ACTION1.ACTIVE 1 --> ACTION1.RUNCOUNT 0
Context
See Actions Table.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.